LP - Cam Latches
This fastener assembly provides basic quarter-turn operation at low installed cost. The plastic studs are combined with a spring steel cam, which is rapidly installed by pushing on to the shaft of the stud. One-way tabs on the cam maintain its position and provide secure stud retention during operation.

- Economical design provides low installed cost
- Slip-on cam adjusts to door thickness, then holds fast
- Grip ranges can be adjusted by adding spacers
- Multiple head styles offer convenient options of hand or tool operation
- Moderate deflection of ramped pawl provides tension for snug closure